Working with our Vertiv Sales team enables complex designs to be configured to your unique needs. If you are an organization seeking technical guidance on a large project, Vertiv can provide the support you require.

Learn More

Many customers work with a Vertiv reseller partner to buy Vertiv products for their IT applications. Partners have extensive training and experience, and are uniquely positioned to specify, sell and support entire IT and infrastructure solutions with Vertiv products.

Find a Reseller

Already know what you need? Want the convenience of online purchase and shipping? Certain categories of Vertiv products can be purchased through an online reseller.


Find an Online Reseller

Need help choosing a product? Speak with a highly qualified Vertiv Specialist who will help guide you to the solution that is right for you.



Contact a Vertiv Specialist

Background

Monash University is a public research university established in Melbourne, Australia in 1958. It offers a large number of courses across numerous disciplines and has a student population of over 70,000. Monash has achieved an enviable national and international reputation for research and teaching excellence in a short 50 years. The University is ranked in the top one per cent of world universities.

Results:

  • Downward trends in power consumption;
  • No need for third party auditing;
  • Cabling costs reduced significantly since the introduction of wireless cables
Case Summary
Location:​

Australia

Vertiv Solution:
  • Trellis™ Thermal System Manager
Critical Needs:

The University’s immediate challenge in its data centre was to reduce cooling costs and mitigate downtime by getting cold air to the areas that needed it the most. Monash had recently experienced small outages due to water leakage, which if left unresolved had the potential to cause serious problems to the overall network. In addition, the University needed a tool that could not only keep pace with the speed and frequency of changes within the infrastructure, but also forecast the environmental impact of changes within the data centre.

Download the Case Study

Related Articles

PARTNERS
Overview
Consultants Corner

Language & Location