Working with our Vertiv Sales team enables complex designs to be configured to your unique needs. If you are an organization seeking technical guidance on a large project, Vertiv can provide the support you require.

Learn More

Many customers work with a Vertiv reseller partner to buy Vertiv products for their IT applications. Partners have extensive training and experience, and are uniquely positioned to specify, sell and support entire IT and infrastructure solutions with Vertiv products.

Find a Reseller

Already know what you need? Want the convenience of online purchase and shipping? Certain categories of Vertiv products can be purchased through an online reseller.


Find an Online Reseller

Need help choosing a product? Speak with a highly qualified Vertiv Specialist who will help guide you to the solution that is right for you.



Contact a Vertiv Specialist

QTS Achieves Higher Energy Efficiency With Upgrades to Vertiv Cooling Systems and Monitoring

April 19, 2021

Background

QTS has experienced significant growth over the past 10 years, going from a single data center in 2005 to a coast-to-coast portfolio of 12 data centers encompassing more than 4.7 million square feet. To ensure continued provision of leading-edge services and optimal performance from its newly acquired facility, QTS required improved cooling system efficiency and greater visibility into system performance. An upgrade of fans and controls, utilizing the latest in cooling technology, was warranted to maintain cooling stability, improve efficiency, and reduce costs.

Results

  • Earned a $150,000 rebate by partnering with Sacramento Municipal Utility District
  • Initially saved $12,000 per month in energy costs and expect additional savings with continued system optimization
  • Reduced carbon footprint with more than 75 percent immediate reduction in the energy consumption of Liebert thermal management units
  • Improved Power Usage Effectiveness (PUE) by 0.16
  • Provided better intelligence to building management system (BMS) for improved system visibility
  • Improved uniformity of under floor static pressure enabling adjustment of air flow to match equipment loads by changing floor tiles
  • Eliminated air leakage through thermal units that were previously off or in standby via the Liebert iCOM control’s proprietary virtual damper
  • Exceeded minimum ROI estimates by 40 percent and achieved targeted savings sooner than budgeted
  • Maximized free cooling through improved unit airflow and cooling control

Case Summary
Location:​ ​Sacramento, California
Critical Need: QTS sought to achieve energy efficiency goals that would deliver enough cost savings to yield a full return on investment (ROI) in 2.5 years. The company also desired advanced monitoring capabilities for continued best-practice data center management.
Vertiv Solution: The team from Vertiv™ Services installed electrically commutated (EC) fans and Liebert® iCOM™ control systems into 64 cooling units, and provided and installed wireless sensors for monitoring of cooling improvements.

DOWNLOAD THE CASE STUDY

PARTNERS
Overview
Consultants Corner

Language & Location