Working with our Vertiv Sales team enables complex designs to be configured to your unique needs. If you are an organization seeking technical guidance on a large project, Vertiv can provide the support you require.

Learn More

Many customers work with a Vertiv reseller partner to buy Vertiv products for their IT applications. Partners have extensive training and experience, and are uniquely positioned to specify, sell and support entire IT and infrastructure solutions with Vertiv products.

Find a Reseller

Already know what you need? Want the convenience of online purchase and shipping? Certain categories of Vertiv products can be purchased through an online reseller.


Find an Online Reseller

Need help choosing a product? Speak with a highly qualified Vertiv Specialist who will help guide you to the solution that is right for you.



Contact a Vertiv Specialist

Vertiv Announces New Rapidly Deployable Additions to Edge Infrastructure Portfolio in Asia

October 22, 2020

Singapore [October 22, 2020] – Vertiv (NYSE: VRT), a global provider of critical digital infrastructure and continuity solutions, today introduced new additions to its portfolio to address growing challenges at the network edge. These products – Vertiv™ VE Rack and the Vertiv™ Edge uninterruptible power supply (UPS) system – are now available in Asia, including Australia and New Zealand.

These latest Vertiv edge infrastructure solutions address the growing demand for flexible, rapidly deployable and highly-efficient solutions as sought by various industries including healthcare, banking, retail, education and manufacturing.

“The current global situation has caused many organizations to rethink their IT deployment strategies and realign their resources from core data centers to edge locations. With this, we’ve noticed that a lot of our customers are now looking for solutions to build their edge sites, starting with high efficiency UPS systems and racks that can be quickly delivered and operational,” said Andy Liu, director for IT and edge infrastructure solutions at Vertiv Asia.

The Vertiv VE rack is an innovative enclosure system that integrates hardware, power management solutions and other peripherals for data centers and computer rooms. Its design allows for easy installation and deployment, with a strong and durable frame that can hold up to 1,600 kilograms of static load. Its 75% perforated door design also allows optimal airflow for efficient heat management, and a variety of tool-less accessories help to facilitate rack management.

The Vertiv Edge is a line-interactive UPS available in mini-tower, rack/tower and rack-mount design configurations, ranging from 500VA to 3,000VA. Designed for small spaces commonly found at the edge, Vertiv Edge UPS features a power factor of 0.9 and extended runtime options, providing high-efficiency power protection for distributed IT at a lower cost.

To learn more about other Vertiv these and other offerings for the edge, visit Vertiv.com/WhatsYourEdgeAsia or Vertiv.com

About Vertiv

Vertiv (NYSE: VRT) brings together hardware, software, analytics and ongoing services to ensure its customers’ vital applications run continuously, perform optimally and grow with their business needs. As Architects of Continuity™, Vertiv solves the most important challenges facing today’s data centers, communication networks and commercial and industrial facilities with a portfolio of power, cooling and IT infrastructure solutions and services that extends from the cloud to the edge of the network. Headquartered in Columbus, Ohio, USA, Vertiv employs approximately 20,000 people and does business in more than 130 countries. For more information, and for the latest news and content from Vertiv, visit Vertiv.com.

CONTACT

Katrina Tirante
T +6326203600 Ext 7666
E Katrina.Tirante@vertiv.com

Reinier Dungca
T +6326203600 Ext 7657
E Reinier.Dungca@vertiv.com

PARTNERS
Overview
Consultants Corner

Language & Location