Working with our Vertiv Sales team enables complex designs to be configured to your unique needs. If you are an organization seeking technical guidance on a large project, Vertiv can provide the support you require.

Learn More

Many customers work with a Vertiv reseller partner to buy Vertiv products for their IT applications. Partners have extensive training and experience, and are uniquely positioned to specify, sell and support entire IT and infrastructure solutions with Vertiv products.

Find a Reseller

Already know what you need? Want the convenience of online purchase and shipping? Certain categories of Vertiv products can be purchased through an online reseller.


Find an Online Reseller

Need help choosing a product? Speak with a highly qualified Vertiv Specialist who will help guide you to the solution that is right for you.



Contact a Vertiv Specialist

Vertiv Introduces Budget-Friendly, Compact Power Protection System for IT Spaces and Edge Applications in Southeast Asia

December 20, 2023

Singapore [December 20, 2023] – Amid growing dependence on technology for either work or play, the need for reliable, cost-effective power protection system also increases. Against this backdrop, Vertiv (NYSE: VRT), a global provider of critical digital infrastructure and continuity solutions, today launched its budget-friendly desktop uninterruptible power supply (UPS) system in select Southeast Asian markets. The Vertiv™ Liebert® PSA-SOHO-LITE is now available in 720VA capacity throughout Southeast Asia, namely Singapore, Malaysia, Vietnam, Indonesia, and Cambodia, and soon in Thailand and Pakistan.

Globe’s newest data center facility in Tiaong improves digital connectivity by widening availability and strengthening reliability of its mobile and fixed network services, resulting in better customer experience. Globe was keen to optimize construction time, while also prioritizing energy efficient operation. Ultimately, this challenge was resolved by Vertiv’s integrated modular solutions, which include Vertiv’s full suite of power, thermal and IT management solutions, and the support of its in-house, in-house expertise in prefabricated data center infrastructure.

The Liebert® PSA-SOHO-LITE is a feature-rich, line-interactive UPS system designed for small IT spaces such as desktop computer workstations, point-of-sale (POS) systems, gaming setup, smart home systems, and other small IT equipment. Compared to other models in its class, the Liebert PSA-SOHO-LITE offers a more compact system, weighing at 4.4 kilograms, but with the same reliable protection against power disturbances provided by the Vertiv™ Liebert® PSA UPS family.

The Liebert PSA-SOHO-LITE comes with fuse protection and built-in automatic voltage regulator (AVR) for clean and stabilized power output. It provides protection against a wide range of power disturbances, including surges, short circuits, overload and over discharge. The Liebert PSA-SOHO-LITE, comes with a newly-designed three-color LED status light, and two universal sockets with ample space for large plugs for convenient connectivity. It also has a built-in overload protection and alarm system for better security.

front 800x450.jpg back-front 800x450.jpg Untitled design.png Untitled design.jpg

“At a time where power protection is critical, having reliable backup power is a must for those working from home or running a small business. That’s why we’re making power protection more accessible to our customers with the release of the new Liebert PSA-SOHO-LITE,” said Andy Liu, director for integrated rack solutions at Vertiv Asia. “The Liebert PSA-SOHO-LITE is suitable for those looking for a UPS alternative that offers efficient protection and reliable backup power support at an affordable cost.”

The Vertiv™ Liebert® PSA-SOHO-LITE is available through Vertiv channel partners and e-commerce stores across select markets in Singapore and Indonesia. To know more about Vertiv’s power protection offerings, visit Vertiv.com.

Learn more about Vertiv’s modular solutions by visiting Vertiv.com.

About Vertiv

Vertiv (NYSE: VRT) brings together hardware, software, analytics and ongoing services to enable its customers’ vital applications to run continuously, perform optimally and grow with their business needs. Vertiv solves the most important challenges facing today’s data centers, communication networks and commercial and industrial facilities with a portfolio of power, cooling and IT infrastructure solutions and services that extends from the cloud to the edge of the network. Headquartered in Westerville, Ohio, USA, Vertiv does business in more than 130 countries. For more information, and for the latest news and content from Vertiv, visit Vertiv.com.

Forward-Looking Statements

This release contains forward-looking statements within the meaning of the Private Securities Litigation Reform Act of 1995, Section 27 of the Securities Act, and Section 21E of the Securities Exchange Act. These statements are only a prediction. Actual events or results may differ materially from those in the forward-looking statements set forth herein. Readers are referred to Vertiv’s filings with the Securities and Exchange Commission, including its most recent Annual Report on Form 10-K and any subsequent Quarterly Reports on Form 10-Q for a discussion of these and other important risk factors concerning Vertiv and its operations. Vertiv is under no obligation to, and expressly disclaims any obligation to, update or alter its forward-looking statements, whether as a result of new information, future events or otherwise.

CONTACT

Katrina Tirante

T +63 2620 3600 ext 7666

E Katrina.Tirante@Vertiv.com

Reinier Dungca

T +63 2620 3600 ext 7657

E Reinier.Dungca@Vertiv.com

PARTNERS
Overview
Consultants Corner

Language & Location