Working with our Vertiv Sales team enables complex designs to be configured to your unique needs. If you are an organization seeking technical guidance on a large project, Vertiv can provide the support you require.

Learn More

Many customers work with a Vertiv reseller partner to buy Vertiv products for their IT applications. Partners have extensive training and experience, and are uniquely positioned to specify, sell and support entire IT and infrastructure solutions with Vertiv products.

Find a Reseller

Already know what you need? Want the convenience of online purchase and shipping? Certain categories of Vertiv products can be purchased through an online reseller.

Find an Online Reseller

Need help choosing a product? Speak with a highly qualified Vertiv Specialist who will help guide you to the solution that is right for you.

Contact a Vertiv Specialist

The German Climate Computing Centre (DKRZ), located in the centre of Hamburg, is renowned by climatologists from around the world.

Here, a team of nearly 80 employees combines technical expertise and special high performance computers to perform complex climate simulations for research purposes. As these simulations require significant computing and data storage capacities, DKRZ has been continuously improving its computing power in order to stay abreast in an evolving and competitive industry. With the installation of a new high performance computing system, Mistral, in summer 2015, DKRZ has seen performance increase twentyfold, at a lower power consumption. The investment into increased computing power and storage capacity has helped to make DKRZ one of the world’s elite computing centres for climate research.

Case Summary
Location:

Hamburg, Germany

Critical Need:

DKRZ was faced with the challenge of upgrading its computing power in an efficient way to ensure reliable and failure-free operations for its new mainframe computer, Mistral. The computer’s energy consumption constantly changes, and can deviate up to 50 percent within fractions of a second. As a result, it was necessary to equip the existing computing centre with a completely new infrastructure, including an uninterruptible power supply (UPS) capable of bridging temporary current fluctuations with ease.

Vertiv Solution:

The Liebert Trinergy Cube configuration at DKRZ is particularly unique. By interconnecting a total of six 400 kVA modules, a single UPS system provides 2400 kVA of power. However, this is only one example of numerous technical advantages which the Liebert Trinergy Cube provides

Download the Case Study

Related Articles

T-Systems Image

Case Studies

T-Systems
PARTNERS
Overview
Consultants Corner
Partner Login

Language & Location