Working with our Vertiv Sales team enables complex designs to be configured to your unique needs. If you are an organization seeking technical guidance on a large project, Vertiv can provide the support you require.

Learn More

Many customers work with a Vertiv reseller partner to buy Vertiv products for their IT applications. Partners have extensive training and experience, and are uniquely positioned to specify, sell and support entire IT and infrastructure solutions with Vertiv products.

Find a Reseller

Already know what you need? Want the convenience of online purchase and shipping? Certain categories of Vertiv products can be purchased through an online reseller.

Find an Online Reseller

Need help choosing a product? Speak with a highly qualified Vertiv Specialist who will help guide you to the solution that is right for you.

Contact a Vertiv Specialist

Vertiv delivers energy-efficient UPS upgrade for ÜNTEL KABLO’s expanding operations

6/10/25

Background

ÜNTEL KABLO is one of the leading cable manufacturers in the world. Established in Turkey in 1972, it has over 50 years of experience of continuously developing and optimizing its product range with the help of advanced technology and well-trained staff. ÜNTEL also manufactures custom products for specialized applications. Today, these products are exported to over 100 countries across six continents.

Results

  • Energy performance: The Vertiv™ Liebert® APM Plus UPS system improved energy efficiency by up to 99% and helped reduce energy consumption, resulting in annual savings, and directly addressing the energy inefficiencies of the previous aging technology.
  • Operational continuity: Modular, hot-swappable architecture helped avoid production downtime during maintenance interventions while reducing service response times through simplified maintenance protocols.
  • Infrastructure scalability: The deployment established a flexible, growth-ready foundation that supports ÜNTEL Kablo's expansion requirements while maintaining optimal energy efficiency and operational reliability.
Case Summary
Location:

Turkey

Vertiv Solution:

Vertiv™ Liebert® APM Plus

DOWNLOAD THE CASE STUDY

Related Articles

Related Links

PARTNERS
Overview
Consultants Corner
Partner Login

Language & Location