Working with our Vertiv Sales team enables complex designs to be configured to your unique needs. If you are an organization seeking technical guidance on a large project, Vertiv can provide the support you require.

Learn More

Many customers work with a Vertiv reseller partner to buy Vertiv products for their IT applications. Partners have extensive training and experience, and are uniquely positioned to specify, sell and support entire IT and infrastructure solutions with Vertiv products.

Find a Reseller

Already know what you need? Want the convenience of online purchase and shipping? Certain categories of Vertiv products can be purchased through an online reseller.

Find an Online Reseller

Need help choosing a product? Speak with a highly qualified Vertiv Specialist who will help guide you to the solution that is right for you.

Contact a Vertiv Specialist

Abstract

“Environmental protection”, “high efficiency” and “energy savings” are nowadays trendy topics and as they also apply to UPS, UPS have become a trendy topic as well. ECO mode represents an interesting feature in UPS technology in particular related to small or single-phase applications with less than 10 kVA. UPS industry has spread its use in the last few years for applications using on-line double conversion products. These products, characterized by double power conversion stages, usually lacked high efficiency performance during on line operation mode, which is why the use of ECO mode brought an extra value to achieve higher efficiency and energy savings. However there is a former ECO mode used inherently in other UPS products and perhaps no so well known: this is exactly the topic we are going to deal with in this paper.

Related Articles

PARTNERS
Overview
Consultants Corner
Partner Login

Language & Location