Working with our Vertiv Sales team enables complex designs to be configured to your unique needs. If you are an organization seeking technical guidance on a large project, Vertiv can provide the support you require.

Learn More

Many customers work with a Vertiv reseller partner to buy Vertiv products for their IT applications. Partners have extensive training and experience, and are uniquely positioned to specify, sell and support entire IT and infrastructure solutions with Vertiv products.

Find a Reseller

Already know what you need? Want the convenience of online purchase and shipping? Certain categories of Vertiv products can be purchased through an online reseller.

Find an Online Reseller

Need help choosing a product? Speak with a highly qualified Vertiv Specialist who will help guide you to the solution that is right for you.

Contact a Vertiv Specialist

Vertiv Offers Scalable Busbar Power Distribution System for Data Centres and Other Dynamic Environments

20/9/22

Vertiv™ Powerbar iMPB enables uninterrupted additions, upgrades and service without using floorspace

London, UK [Sept. 20, 2022] – Vertiv (NYSE: VRT), a global provider of critical digital infrastructure and continuity solutions, continues the expansion of its power distribution portfolio with the availability of Vertiv™ Powerbar iMPB, a modular busbar system designed to enable seamless, on-demand power upgrades in dynamic data centre environments. Available in both copper and aluminium conductor offerings, the Vertiv Powerbar iMPB family features capacities from 160 amps to 1,000 amps and delivers reliable overhead power distribution, with the inherent benefit of also maximising cooling airflow. The system is ideal for use in almost any size or style of data centre, as well as laboratories, distribution warehouses, adaptable manufacturing plants and other dynamic environments. The Vertiv Powerbar iMPB is available in North America, Latin America, Asia – including Australia and New Zealand, India, Europe, the Middle East and Africa.

The busway system allows businesses to cost-effectively optimise and adapt power distribution infrastructure over time, maximising availability through continuous power delivery to critical loads. User-friendly tap-off boxes with breaker protection can be placed anywhere along the busway and isolate active IT loads and nearby branch breakers to ensure continuous power delivery. The adaptive busbar comes with a simple sandwich-style joint pack construction that makes installation secure and easy, with no special tooling required. The Vertiv Powerbar iMPB includes a variety of capacity and connection configurations to allow for adjustments and upgrades with minimal outside support and no loss of power to critical loads.

“As more and more devices are added and higher rack densities become commonplace, space is at a premium in today’s data centres,” said Phil O’Doherty, managing director, E&I at Vertiv. “The power infrastructure must keep pace, which means being scalable and quick to deploy. The Vertiv Powerbar iMPB delivers on all fronts with a modular, easy-to-install system that is compact and flexible enough to meet constantly changing demands.”

The Vertiv™ Powerbar iMPB is UL 857 and IEC 61439-2 compliant, and the lightweight aluminium busway track chassis has an IP2X/3X safety rating with integrated finger-safe capabilities and ground-first/break-last design to ensure maximum safety while servicing. With both copper and recyclable aluminium conductor options, the busbar can be configured to meet the conductivity and safety requirements of any installation.

The Vertiv Powerbar iMPB, a mature offering from Vertiv’s E&I brand, will supersede the previous Vertiv™ Liebert® MBX busway product that was available in North America and EMEA, and is compatible with the previous offering. The Vertiv Powerbar iMPB solution complements the Vertiv™ E&I switchgear range to provide a complete power distribution solution.

For more information about the Vertiv Powerbar iMPB and other data centre power solutions, visit Vertiv.com.

About Vertiv

Vertiv (NYSE: VRT) brings together hardware, software, analytics and ongoing services to enable its customers’ vital applications to run continuously, perform optimally and grow with their business needs. Vertiv solves the most important challenges facing today’s data centres, communication networks and commercial and industrial facilities with a portfolio of power, cooling and IT infrastructure solutions and services that extends from the cloud to the edge of the network. Headquartered in Columbus, Ohio, USA, Vertiv employs approximately 24,000 people and does business in more than 130 countries. For more information, and for the latest news and content from Vertiv, visit Vertiv.com.

Forward-Looking Statements

This release contains forward-looking statements within the meaning of the Private Securities Litigation Reform Act of 1995, Section 27 of the Securities Act, and Section 21E of the Securities Exchange Act. These statements are only a prediction. Actual events or results may differ materially from those in the forward-looking statements set forth herein. Readers are referred to Vertiv’s filings with the Securities and Exchange Commission, including its most recent Annual Report on Form 10-K and any subsequent Quarterly Reports on Form 10-Q for a discussion of these and other important risk factors concerning Vertiv and its operations. Vertiv is under no obligation to, and expressly disclaims any obligation to, update or alter its forward-looking statements, whether as a result of new information, future events or otherwise.

CONTACT

Susanna Collins

T +44(0)7872 558593
E susanna.collins@apodpr.co.uk

Related Articles

E+I Image

Articles

E+I
PARTNERS
Overview
Consultants Corner
Partner Login

Language & Location