Working with our Vertiv Sales team enables complex designs to be configured to your unique needs. If you are an organization seeking technical guidance on a large project, Vertiv can provide the support you require.

Learn More

Many customers work with a Vertiv reseller partner to buy Vertiv products for their IT applications. Partners have extensive training and experience, and are uniquely positioned to specify, sell and support entire IT and infrastructure solutions with Vertiv products.

Find a Reseller

Already know what you need? Want the convenience of online purchase and shipping? Certain categories of Vertiv products can be purchased through an online reseller.


Find an Online Reseller

Need help choosing a product? Speak with a highly qualified Vertiv Specialist who will help guide you to the solution that is right for you.



Contact a Vertiv Specialist

Vertiv to Expand Cutting-edge Customer Experience Centre

September 29, 2020

New investments will further enhance uninterruptible power supply testing capabilities for Vertiv customers worldwide

Castel Guelfo, Bologna [February 6, 2020] – Vertiv, a global provider of critical infrastructure and continuity solutions, today announced plans to start expansion of its state-of-the-art AC Power Customer Experience Centre in Bologna, Italy in early 2020. The construction plan will include a new, 4 MVA power infrastructure to bolster testing capabilities, flexibility and efficiency. This enhancement aids in addressing the trend towards bigger data centers and industrial plants, and the growing customer demand for extended offsite pre-testing to speed up site deployments.

As a leading provider of data centre hardware, software, analytics and ongoing services, Vertiv counts 70% of Fortune 500 companies among its customer base. The Customer Experience Centre offers these companies a front row seat to the work being done to protect their critical data infrastructure and allows them to witness the testing of a variety of power conditions.

The planned enhancements to the Customer Experience Centre will more than double the testing capacity currently available for large Uninterruptible Power Supplies (UPS), offering up to 7,5 MVA of power and the capability to host six simultaneous sessions. The facility is already able to perform safe capacity tests utilizing regenerative loads with a power-loop principle, to avoid unnecessary energy waste and re-use about 96% of energy. More efficient and thorough testing, including dynamic tests on batteries, an advanced DC simulator to replicate any kind of battery set-up, and the ability to test 480V systems are also central benefits of the planned expansion. The enhancements will create a comprehensive AC Power testing facility where customers from all over the world can witness advanced technology solutions and latest innovations, as well as verify the performance of Vertiv systems simulating real site operating conditions.

This planned investment comes six years after the opening of the Customer Experience Centre. At the time of opening, it was the only facility in Europe that was purpose-built for the validation of data centre infrastructure, allowing customers to witness pre-installation demonstrations covering the technical performance, interoperability and efficiency of UPS systems under real-field conditions. To this day, the facility enables Vertiv customers and prospects to experience first-hand a wide variety of technologies, supported by constant consultation from research and development (R&D) and engineering specialists.

Andrea Ferro, director of the AC Power line of business for Europe, Middle East and Africa at Vertiv, says: “The centre was pioneering when it opened six years ago and continues to drive innovation today. The latest investment is testament to Vertiv’s commitment to our growing customer base, as it will allow us to conduct more tests simultaneously. The unique opportunity to personally prove the reliability and cost-effectiveness of Vertiv products under a range of real-life conditions helps enable peace of mind for our customers."

The expansion of the facility is planned to be completed by 2021, with the first phase starting in early 2020. For more information on Vertiv’s AC Power products and Customer Experience Centres, visit Vertiv.com.

About Vertiv

Vertiv brings together hardware, software, analytics and ongoing services to ensure its customers’ vital applications run continuously, perform optimally and grow with their business needs. Vertiv solves the most important challenges facing today’s data centres, communication networks and commercial and industrial facilities with a portfolio of power, cooling and IT infrastructure solutions and services that extends from the cloud to the edge of the network. Headquartered in Columbus, Ohio, USA, Vertiv employs around 20,000 people and does business in more than 130 countries. For more information, and for the latest news and content from Vertiv, visit Vertiv.com.

Media Contact

Katie Evans 
Tel. +44(0)20 3997 8367
E-mail: katie.evans@madebychameleon.com

Related Articles

PRODUCTS & SERVICES
Overview
PARTNERS
Overview
Consultants Corner
PARTNERS
Overview
Consultants Corner
Partner Login

Language & Location