Working with our Vertiv Sales team enables complex designs to be configured to your unique needs. If you are an organization seeking technical guidance on a large project, Vertiv can provide the support you require.

Learn More

Many customers work with a Vertiv reseller partner to buy Vertiv products for their IT applications. Partners have extensive training and experience, and are uniquely positioned to specify, sell and support entire IT and infrastructure solutions with Vertiv products.

Find a Reseller

Already know what you need? Want the convenience of online purchase and shipping? Certain categories of Vertiv products can be purchased through an online reseller.


Find an Online Reseller

Need help choosing a product? Speak with a highly qualified Vertiv Specialist who will help guide you to the solution that is right for you.



Contact a Vertiv Specialist

Vertiv announces global launch of chilled water rear door heat exchanger for AI and HPC applications

18/3/25

Vertiv™ CoolLoop RDHx delivers energy-efficient rack cooling, complementing direct-to-chip liquid cooling and optimizing heat dissipation for high-density IT and AI environments.

Columbus, Ohio [March 18, 2025] – Vertiv (NYSE: VRT), a global provider of critical digital infrastructure and continuity solutions, today announced the launch of the Vertiv™ CoolLoop RDHx, a chilled water, high density rear door heat exchanger (RDHx) designed to support the increasing thermal demands of AI, high-performance computing (HPC), and other power-dense IT workloads. Now available globally in capacities up to 80kW per rack, the solution is an extension of the Vertiv™ Liebert® DCD rear door heat exchanger family and part of Vertiv’s industry-leading thermal management portfolio.

The Vertiv CoolLoop RDHx is a compact, energy-efficient air-cooling door replacement that may be deployed as a standalone solution or can support direct-to-chip liquid cooling for a room-neutral solution. The system’s integrated fan module delivers precise airflow control, reducing energy consumption while optimizing cooling performance.

The Vertiv CoolLoop RDHx offers key features that enhance adaptability and efficiency in diverse rack configurations.

  • Modular compatibility allows installation on 600mm and 800mm-wide IT racks, with optional height adapters available for flexible deployment.
  • Primary and secondary cooling circuit integration enables both the connection to the primary cooling networks and the connection to liquid cooling infrastructure, enhancing system-wide thermal efficiency.
  • Pressure-independent control valve option provides precise regulation of chilled water flow, optimizing cooling performance.

"As liquid cooling is adopted to remove heat from AI servers, it’s necessary to find a streamlined solution to eliminate the additional air loaded heat," said Nigel Gore, vice president of high- density liquid cooling at Vertiv. "The Vertiv™ CoolLoop RDHx features a space-saving rear-door configuration and integrates seamlessly with the liquid cooling loop, simplifying heat dissipation while maintaining efficiency and scalability for high-density environments."

Vertiv CoolLoop RDHx can be supported by Vertiv™ Liquid Cooling Services, a new offering portfolio that provides comprehensive lifecycle support for the entire liquid cooling ecosystem, from design and installation to maintenance and fluid management.

For more information on Vertiv CoolLoop RDHx, the expanding liquid cooling portfolio, Vertiv Liquid Cooling Services, or Vertiv’s industry-leading cooling solutions, visit Vertiv.com.

About Vertiv

Vertiv (NYSE: VRT) brings together hardware, software, analytics and ongoing services to enable its customers’ vital applications to run continuously, perform optimally and grow with their business needs. Vertiv solves the most important challenges facing today’s data centers, communication networks and commercial and industrial facilities with a portfolio of power, cooling and IT infrastructure solutions and services that extends from the cloud to the edge of the network. Headquartered in Westerville, Ohio, USA, Vertiv does business in more than 130 countries. For more information, and for the latest news and content from Vertiv, visit Vertiv.com.

Forward-Looking Statements

This release contains forward-looking statements within the meaning of the Private Securities Litigation Reform Act of 1995, Section 27 of the Securities Act, and Section 21E of the Securities Exchange Act. These statements are only a prediction. Actual events or results may differ materially from those in the forward-looking statements set forth herein. Readers are referred to Vertiv’s filings with the Securities and Exchange Commission, including its most recent Annual Report on Form 10-K and any subsequent Quarterly Reports on Form 10-Q for a discussion of these and other important risk factors concerning Vertiv and its operations. Vertiv is under no obligation to, and expressly disclaims any obligation to, update or alter its forward-looking statements, whether as a result of new information, future events or otherwise.

 

CONTACT
Ruder Finn
E Vertiv@RuderFinn.com

Related Articles

PARTNERS
Partner Login

Language & Location