Working with our Vertiv Sales team enables complex designs to be configured to your unique needs. If you are an organization seeking technical guidance on a large project, Vertiv can provide the support you require.

Learn More

Many customers work with a Vertiv reseller partner to buy Vertiv products for their IT applications. Partners have extensive training and experience, and are uniquely positioned to specify, sell and support entire IT and infrastructure solutions with Vertiv products.

Find a Reseller

Already know what you need? Want the convenience of online purchase and shipping? Certain categories of Vertiv products can be purchased through an online reseller.


Find an Online Reseller

Need help choosing a product? Speak with a highly qualified Vertiv Specialist who will help guide you to the solution that is right for you.



Contact a Vertiv Specialist

What is accelerated computing?

Data plays an increasingly central role in innovation and decision-making, so the demand for advanced computing solutions has never been higher. From artificial intelligence (AI) and machine learning (ML) to big data analytics and scientific research, organizations are handling and generating more data than ever, leading to the rise of accelerated computing. 

Accelerated computing is a technology that utilizes specialized processors, such as graphics processing units (GPUs), to perform complex computational tasks at a faster rate than traditional central processing units (CPUs).  

This article explains how accelerated computing is shaping the future of these fields by enabling more rapid and effective data handling and analysis. We will also discuss the power and cooling challenges in accelerated computing and how Vertiv’s solutions address them to support its optimal operation. 

Understanding accelerated computing

CPUs excel at handling sequential tasks but need help with the highly parallel nature of AI data centers and complex simulations. This is where accelerated computing steps in. It utilizes specialized hardware, called accelerators, that work alongside CPUs to significantly boost processing power and speed. These accelerators are designed to tackle specific workloads much faster and more efficiently than CPUs, enabling groundbreaking advancements in various fields. 

At its core, accelerated computing leverages specialized hardware to offload demanding computational tasks from CPUs. These accelerators, like Graphics Processing Units (GPUs), Tensor Processing Units (TPUs), and Field-Programmable Gate Arrays (FPGAs), are built with parallel processing in mind. Parallel processing involves performing multiple computations simultaneously. To illustrate, it is like having multiple lanes on a highway instead of just one, leading to a significant performance boost. 

Benefits of accelerated computing

Accelerated computing provides many advantages, significantly improving performance and efficiency across various applications:

  • Faster processing: Accelerated computing dramatically reduces processing times, enabling real-time analysis and faster decision-making. 

  • Increased efficiency: Accelerated computing utilizes resources more effectively and reduces overall energy consumption by offloading tasks to specialized hardware. 

  • Cost-effectiveness: The faster processing times and improved efficiency translate to significant cost savings for businesses. 

  • Unlocking innovation: Accelerated computing empowers researchers, data scientists, and developers to tackle complex problems and unlock groundbreaking advancements in AI, big data, and scientific discovery. 

Specialized hardware accelerators 

The key to accelerated computing lies in understanding the role of various hardware accelerators. These accelerators are designed to handle specific types of computations more efficiently than general-purpose CPUs, offering significant performance and energy efficiency improvements.

Here’s an overview of the most prominent types of hardware accelerators and their unique benefits:  

1. Graphics Processing Units (GPUs)  

Initially developed for rendering graphics in video games, GPUs are optimized for parallel processing, making them well-suited for tasks like image and video processing, deep learning, AI computing, and scientific simulations across various fields such as physics, chemistry, and biology.

2. Tensor Processing Units (TPUs)  

TPUs, or Tensor Processing Units, are specialized hardware developed by Google for machine learning tasks, particularly those involving neural networks. They are designed to perform machine learning operations efficiently, offering optimized neural network performance, energy efficiency, and scalability through Google's cloud infrastructure without the high initial costs associated with hardware investment.

3. Field-Programmable Gate Arrays (FPGAs) 

FPGAs are unique hardware accelerators due to their reconfigurability, offering customization, low latency, and energy efficiency. They can be tailored for specific applications, execute tasks with low latency, and achieve high performance with lower power consumption. 

4. Application-Specific Integrated Circuits (ASICs)  

ASICs are chips custom-designed for specific tasks, offering high performance and energy efficiency over general-purpose hardware. They are ideal for tasks like cryptocurrency mining due to their speed and minimal power consumption. Although ASICs have a higher initial development cost, their efficiency makes them cost-effective for large-scale use. Unlike FPGAs, ASICs perform a fixed function, avoiding the overhead of reprogrammable logic. 

5. Digital Signal Processors (DSPs)  

DSPs are specialized microprocessors optimized for real-time processing of digital signals. They are used in applications such as audio/video processing, telecommunications, and sensor data analysis. Capable of high-speed numerical operations, DSPs efficiently handle continuous data streams and are commonly found in embedded systems, offering power-efficient computation.

6. Hybrid Accelerators  

As demand for diverse computational tasks grows, hybrid accelerators combining CPUs, GPUs, FPGAs, and other specialized hardware are emerging. These systems optimize performance for a wide range of applications, leveraging different processors to maximize efficiency and scalability. Specialized hardware accelerators like GPUs, TPUs, FPGAs, ASICs, and DSPs each bring unique strengths to the table, enabling innovation and transforming data processing and analysis across industries.

Where is accelerated computing used? 

Accelerated computing is reshaping numerous industries by facilitating the rapid and efficient execution of complex and data-intensive tasks. Here are some use cases:

a. Artificial intelligence and machine learning  

AI and machine learning applications require massive computational power to process large datasets and train complex models. GPUs and TPUs accelerate these processes, enabling faster training times and more accurate models. This capability is essential for natural language processing, image recognition, and predictive analytics applications.

b. Big data analytics  

Organizations across industries collect vast amounts of data. Analyzing this data in real-time requires significant computational resources. Accelerated computing allows for the rapid processing of big data, providing timely insights to drive business decisions. This is particularly useful in finance, healthcare, and retail sectors. 

c. Scientific research  

In scientific fields, accelerated computing facilitates complex simulations and data analysis. For example, in genomics, accelerated computing helps process genetic data quickly, aiding in research and personalized medicine. Similarly, in physics, it enables simulations of complex phenomena, such as particle interactions. 

d. Autonomous vehicles  

Self-driving cars rely on accelerated computing to process data from various sensors in real-time. This data includes information from cameras, lidar, and radar, which must be analyzed quickly to make split-second driving decisions. GPUs enable the high-speed computations required for safe and efficient autonomous driving. 

e. Financial services

In the financial industry, accelerated computing supports high-frequency trading, risk management, and fraud detection. These applications require real-time data analysis and complex algorithmic computations, which GPUs and FPGAs efficiently handle.

Infrastructure challenges and solutions 

1. Power distribution and management: 
  • Challenge: High power density requirements of GPUs and TPUs increase demands on power distribution systems, leading to potential inefficiencies and increased operational costs.

  • Solution: Deploying high-efficiency power supplies and voltage regulators minimizes power loss, improves energy efficiency, and ensures stable power delivery to accelerated computing hardware. Advanced power monitoring and management tools optimize power usage and identify opportunities for efficiency improvements.

2. Cooling systems:
  • Challenge: Accelerated computing hardware generates significant heat, requiring robust cooling solutions to prevent thermal issues and maintain optimal operating conditions.

  • Solution: Implementing advanced cooling technologies such as liquid cooling or direct-to-chip cooling efficiently dissipates heat, enhances cooling capacity, and minimizes the risk of hardware overheating. Environmental monitoring systems continuously assess conditions and adjust cooling strategies to optimize efficiency.

3. Space and layout optimization:
  • Challenge: Accommodating the physical footprint and heat dissipation requirements of GPUs and TPUs within existing data center infrastructure can be challenging.

  • Solution: Optimizing data center layout and rack configurations to support higher power densities and airflow requirements. Modular infrastructure designs facilitate flexible expansion and scalability while maintaining efficient cooling and operational reliability. Efficient cable management practices reduce airflow obstructions and enhance cooling effectiveness.

4. Infrastructure efficiency and sustainability:
  • Challenge: High energy consumption and environmental impact associated with accelerated computing operations.
  • Solution: Selecting energy-efficient hardware and integrating renewable energy sources like solar or wind power reduces overall carbon footprint and operational costs. Optimizing Power Usage Effectiveness (PUE) through hardware optimization, virtualization, and workload consolidation improves energy efficiency metrics.
5. Scalability and future-readiness:
  • Challenge: Scaling accelerated computing infrastructure while maintaining performance, efficiency, and cost-effectiveness.

  • Solution: Designing flexible infrastructure that supports modular expansion and integrates future hardware advancements seamlessly. Predictive analytics tools forecast infrastructure needs and optimize resource allocation, enabling proactive planning for capacity expansions and upgrades. Collaborating with vendors ensures alignment with emerging technologies and industry trends, supporting long-term scalability and innovation.

By addressing these challenges with the recommended hardware and system solutions, modern data centers can optimize their accelerated computing environments for improved performance, efficiency, and reliability, thereby enabling continued innovation and growth in high-performance computing applications.

Implementation obstacles: Beyond the hardware 

While the benefits of accelerated computing are undeniable, implementing it effectively comes with its own set of challenges:

Compatibility and installation issues 

Implementing accelerated computing in existing infrastructure can be challenging due to compatibility and installation issues. Many data centers are built around traditional CPUs, and integrating specialized hardware accelerators requires careful planning and execution. Ensuring compatibility with existing systems and software is essential to avoid disruptions and maximize performance gains. 

Need for specialized tools and software 

Beyond hardware, accelerated computing often necessitates specialized tools and software to fully leverage the capabilities of hardware accelerators. This includes optimized libraries, frameworks, and development environments tailored for GPUs, TPUs, and FPGAs. Navigating this ecosystem can be daunting without the right expertise and resources. 

Accelerated computing: Partner for power, efficiency, and innovation

Accelerated computing is transforming industries with its enhanced data processing capabilities, but it brings challenges like heat management and infrastructure scalability. To navigate these complexities effectively, consult a Vertiv expert for tailored solutions in power distribution, advanced cooling, and infrastructure optimization. 

Related Articles

PARTNERS
PARTNERS
Partner Login

Language & Location