Working with our Vertiv Sales team enables complex designs to be configured to your unique needs. If you are an organization seeking technical guidance on a large project, Vertiv can provide the support you require.

Learn More

Many customers work with a Vertiv reseller partner to buy Vertiv products for their IT applications. Partners have extensive training and experience, and are uniquely positioned to specify, sell and support entire IT and infrastructure solutions with Vertiv products.

Find a Reseller

Already know what you need? Want the convenience of online purchase and shipping? Certain categories of Vertiv products can be purchased through an online reseller.


Find an Online Reseller

Need help choosing a product? Speak with a highly qualified Vertiv Specialist who will help guide you to the solution that is right for you.



Contact a Vertiv Specialist

Vertiv Introduces New Scalable Inverter
System that Saves Space and Minimizes
Energy Loss for Edge, Core and Access
Site Applications in the Americas

October 30, 2023

Vertiv™ NetSure™ Inverter System powers AC loads in a compact footprint with zero transfer time from grid to battery

Columbus, Ohio [October 30, 2023] – Vertiv (NYSE: VRT), a global provider of critical digital infrastructure and continuity solutions, today introduced new models of the Vertiv™ NetSure™ Inverter System, scalable, modular, inverters that save space and improve reliability for DC-based applications. The new NetSure™ Integrated Inverter model is a single sub-rack with a common battery bank that powers both AC and DC loads. The Netsure™ Stand-Alone model provides AC output from an existing DC power system and batteries. The inverter systems are designed for DC applications requiring AC output for applications, often Information and Communications Technology (ICT) telecom sites that include servers, switches, routers, firewalls, lighting, and security systems. The new models are available today in the Americas with 120 VAC output.

Telecom site challenges typically include limited space, critical availability, and the need for high efficiency. The NetSure Inverter System addresses all of these issues: compact systems and use of a common battery bank minimize required footprint; zero transfer time from grid to battery contributes to reliable operation; and inverter modules that operate at up to 95.2% efficiency, reducing costly electricity bills and emissions of greenhouse gasses.  

The fully integrated NetSure Integrated Inverter System provides DC and AC power from a common platform using a single control unit, eliminating the need for separate controllers for the DC power system and the inverter. This system includes AC and DC distribution, Vertiv™ eSure™ rectifiers and inverters, and a shared battery bank. Working in concert, the system provides zero transfer time between AC mains and DC battery sources, delivering reliable backup for critical loads from 5kVA to 12kVA. The Vertiv™ NetSure™ Control Unit monitors both AC inverters and DC rectifiers, requiring no investment in additional controls, while eliminating the space required for separate systems and batteries, and reducing the need for separate maintenance programs for the traditional configuration. By providing clear visibility into both AC and DC loads, it enables more accurate capacity planning and management, and maximum availability. 

The Vertiv™ NetSure™ Stand-Alone Inverter System leverages a site’s existing DC power infrastructure and batteries, supporting critical AC loads from 5kVA to 24kVA, and maximizing site availability with zero transfer time from grid to battery. The Vertiv™ NetSure™ eSure™ inverters may be managed locally or remotely with the NetSure™ Control Unit.

Both NetSure™ Inverter Systems are available in 19” or 23” mounting widths. Energy efficiencies are up to 95.2% across a wide operating range, and inverter power densities are market-leading in its class at 19VA/in3.

“As technology adoption expands and mobile devices are increasingly a lifeline for personal and business activities, more computing is introduced into traditional DC-powered environments, including access sites and edge deployments. The need to reliably and efficiently manage both AC and DC loads increases,” said Henrik Nilén, director of global DC power offerings for Vertiv. “With a single battery bank supporting both AC and DC loads and market-leading inverter power density in its class, the NetSure Inverter System is designed to optimize space and enable outstanding site availability.”

Vertiv has a long history in both AC and DC power, with broad portfolios of AC-powered IT infrastructure solutions and DC-powered telecom infrastructure solutions. That deep expertise was critical to the development of the NetSure Inverter Series. Vertiv™ DC Power Services engineering, installation, project management, and maintenance teams are available to support all DC power applications, regardless of manufacturer.

For more information on the Vertiv NetSure Inverter System or the full portfolio of data center and telecommunications infrastructure solutions from Vertiv, visit Vertiv.com.

 

About Vertiv

Vertiv (NYSE: VRT) brings together hardware, software, analytics and ongoing services to enable its customers’ vital applications to run continuously, perform optimally and grow with their business needs. Vertiv solves the most important challenges facing today’s data centers, communication networks and commercial and industrial facilities with a portfolio of power, cooling and IT infrastructure solutions and services that extends from the cloud to the edge of the network. Headquartered in Westerville, Ohio, USA, Vertiv does business in more than 130 countries. For more information, and for the latest news and content from Vertiv, visit Vertiv.com. 

Forward-Looking Statements

This release contains forward-looking statements within the meaning of the Private Securities Litigation Reform Act of 1995, Section 27 of the Securities Act, and Section 21E of the Securities Exchange Act. These statements are only a prediction. Actual events or results may differ materially from those in the forward-looking statements set forth herein. Readers are referred to Vertiv’s filings with the Securities and Exchange Commission, including its most recent Annual Report on Form 10-K and any subsequent Quarterly Reports on Form 10-Q for a discussion of these and other important risk factors concerning Vertiv and its operations. Vertiv is under no obligation to, and expressly disclaims any obligation to, update or alter its forward-looking statements, whether as a result of new information, future events or otherwise. 

CONTACT

Sara Steindorf
T +314-982-1725
E sara.steindorf@fleishman.com

 

Related Articles

PARTNERS
Overview
Consultants Corner
PARTNERS
Overview
Consultants Corner
MY ACCOUNT
Overview
Partner Login

Language & Location