Working with our Vertiv Sales team enables complex designs to be configured to your unique needs. If you are an organization seeking technical guidance on a large project, Vertiv can provide the support you require.

Learn More

Many customers work with a Vertiv reseller partner to buy Vertiv products for their IT applications. Partners have extensive training and experience, and are uniquely positioned to specify, sell and support entire IT and infrastructure solutions with Vertiv products.

Find a Reseller

Already know what you need? Want the convenience of online purchase and shipping? Certain categories of Vertiv products can be purchased through an online reseller.


Find an Online Reseller

Need help choosing a product? Speak with a highly qualified Vertiv Specialist who will help guide you to the solution that is right for you.



Contact a Vertiv Specialist

Vertiv expands liquid cooling portfolio to make North America AI deployments easier, faster and more cost-effective

October 07, 2024

Vertiv™ CoolPhase CDU and Vertiv™ CoolChip Fluid Network rack manifold overcome traditional barriers to the introduction of liquid cooling in data centers

COLUMBUS, Ohio [October 7, 2024] – Vertiv (NYSE: VRT), a global provider of critical digital infrastructure and continuity solutions, today announced a significant expansion of the Vertiv™ liquid cooling product portfolio with the introduction of the Vertiv™ CoolPhase CDU liquid-to-refrigerant coolant distribution unit and Vertiv™ CoolChip Fluid Network in-rack manifold. These systems enable modular, cost-effective liquid cooling deployments in data centers that weren’t originally configured for liquid cooling, making it possible to deploy high-density computing for AI alongside traditional air-cooled racks. The new systems are available now in North America.

The Vertiv CoolChip family delivers much-needed flexibility to data centers and colocation providers and enables fast, modular growth to support the increasing demand for AI deployments. Along with these new systems, Vertiv has a full suite of global service offerings to support the deployment of liquid cooled infrastructure, ranging from solution design to installation to on-going lifecycle management.

The Vertiv™ CoolPhase CDU is a liquid-to-refrigerant coolant distribution unit that uniquely offers direct to chip liquid cooling support with refrigerant-based heat rejection, enabling it to easily retrofit into existing facilities and to deploy liquid cooling in direct-to-chip applications without a facility chilled water system.  The system can be rapidly deployed without the need for complex chilled water loops. The system can distribute coolant directly to chips, rear-door heat exchangers or even other CDUs, with full control of different and elevated temperature settings, eliminating multiple heat exchange loops. Combined with Vertiv™ EconoPhase technology and variable speed pumps, the system delivers free-cooling and enhances overall data center efficiency. The system leverages teamwork system level control, dual or triple power supplies for high availability; remote temperature, humidity and leak detection sensors; and integrated controls that enable remote monitoring and management.

Vertiv™ CoolPhase CDU can be deployed standalone to support liquid cooling loads or combined as part of the Vertiv™ Liebert® DSE room-based air cooling system as a complete thermal chain to support a hybrid air and liquid cooled environment.

The Vertiv™ CoolChip Fluid Network in-rack manifold is mounted in the zero-U space of industry-standard racks to route fluid from the coolant distribution unit to the server. With multiple coupling sizes, top or bottom dripless quick connects, and various port quantity combinations, the Vertiv CoolChip Fluid Network is easily installed and can be tailored to any direct-to-chip liquid cooling application.

“The proliferation of AI can only happen with the support of advanced cooling technologies,” said John Niemann, senior vice president of the thermal business unit at Vertiv. “Vertiv’s new liquid-cooled solutions and services enable both new and existing data centers to seamlessly introduce liquid cooling, making AI deployments easier, faster and more cost-effective than traditional approaches.”

For more information on the thermal management portfolio or other Vertiv solutions for modern data centers, visit Vertiv.com.

About Vertiv

Vertiv (NYSE: VRT) brings together hardware, software, analytics and ongoing services to enable its customers’ vital applications to run continuously, perform optimally and grow with their business needs. Vertiv solves the most important challenges facing today’s data centers, communication networks and commercial and industrial facilities with a portfolio of power, cooling and IT infrastructure solutions and services that extends from the cloud to the edge of the network. Headquartered in Westerville, Ohio, USA, Vertiv does business in more than 130 countries. For more information, and for the latest news and content from Vertiv, visit Vertiv.com.

Forward-Looking Statements

This release contains forward-looking statements within the meaning of the Private Securities Litigation Reform Act of 1995, Section 27 of the Securities Act, and Section 21E of the Securities Exchange Act. These statements are only a prediction. Actual events or results may differ materially from those in the forward-looking statements set forth herein. Readers are referred to Vertiv’s filings with the Securities and Exchange Commission, including its most recent Annual Report on Form 10-K and any subsequent Quarterly Reports on Form 10-Q for a discussion of these and other important risk factors concerning Vertiv and its operations. Vertiv is under no obligation to, and expressly disclaims any obligation to, update or alter its forward-looking statements, whether as a result of new information, future events or otherwise.

 

CONTACT

Brianna Rabe - Ruder Finn
E brianna.rabe@ruderfinn.com

PARTNERS
Overview
Consultants Corner
PARTNERS
Overview
Consultants Corner
MY ACCOUNT
Overview
Partner Login

Language & Location