Working with our Vertiv Sales team enables complex designs to be configured to your unique needs. If you are an organization seeking technical guidance on a large project, Vertiv can provide the support you require.

Learn More

Many customers work with a Vertiv reseller partner to buy Vertiv products for their IT applications. Partners have extensive training and experience, and are uniquely positioned to specify, sell and support entire IT and infrastructure solutions with Vertiv products.

Find a Reseller

Already know what you need? Want the convenience of online purchase and shipping? Certain categories of Vertiv products can be purchased through an online reseller.


Find an Online Reseller

Need help choosing a product? Speak with a highly qualified Vertiv Specialist who will help guide you to the solution that is right for you.



Contact a Vertiv Specialist

Language models, explained: How Natural Language Processing (NLP) works

This article aims to demystify language models, shedding light on their foundational concepts and mechanisms for processing raw text data. It covers several types of language models and large language models, focusing on Neural Network-Based models and delving into the intricate workings of transformers, notably BERT by Google. We also explore the exciting future of language models, including potential trends shaping its evolution. 

Language model definition

A Language Model focuses on the ability to generate human-like text. A general language model is fundamentally a statistical model or probability distribution over sequences of words, deciphering the likelihood of words occurring in each sequence. This helps predict the next word or words based on the preceding words in a sentence.

A simple probabilistic language model can be used in various applications such as machine translation, autocorrect, voice recognition, and autocomplete features to fill in the following word for the user or suggest possible word sequences.

Such models have evolved with more advanced models, including transformer models like BERT, providing more accurate predictions of the next word by considering surrounding words and context across the entire text rather than focusing merely on the previous word or previous words in the sequence.

How do language models relate to artificial intelligence

Language models are intimately tied to computer science and Artificial Intelligence (AI), serving as the foundation of Natural Language Processing (NLP), a crucial sub-discipline of AI. The primary objective of AI is to emulate human intelligence. Language - a defining characteristic of human cognition - is indispensable to this endeavor.

A good language model aims to comprehend and generate human-like text, enabling machine learning where machines understand context, sentiment, and semantic relationships between words, including grammar rules and parts of speech, emulating human-like comprehension.

This type of machine learning ability is a significant step toward achieving true AI, facilitating human-computer interaction in natural language, and enabling machines to perform complex NLP tasks that involve understanding and generating human language. This includes modern natural language processing tasks like translation, speech recognition, and sentiment analysis.

Reading the raw text corpus

Before diving into the mechanisms and feature functions employed by language models, it's essential to understand how they grapple with raw text corpus - the unstructured data upon which a statistical model is trained. The initial step in language modeling involves reading this fundamental text corpus, or what can be considered the conditioning context of the model. This core component of the model can be composed of anything from literary works to web pages or even transcriptions of spoken language. Regardless of its origins, this corpus represents the richness and complexity of language in its rawest form. The scope and breadth of the corpus or textural data set used for the training classify an AI language model as a large language model.

A language model learns by reading the conditioning context or text corpus word by word, sentence by sentence, capturing the intricate underlying structure and patterns within the language. It does this by encoding the words into numerical vectors - a process known as word embedding. These vectors meaningfully represent words, encapsulating their semantic and syntactic properties. For instance, words used in similar contexts tend to have similar vectors. Model processes that convert words into vectors are crucial because they allow language models to manipulate language in a mathematical format, paving the way for the prediction of word sequences and enabling more advanced processes like translation and sentiment analysis.

Having read and encoded the raw text corpus, language models are primed to generate human-like text or predict word sequences. The mechanisms employed for these NLP tasks vary from model to model. Still, they all share a common underlying goal - deciphering the probability of a given sequence occurring in real life. This will be discussed further in the coming section.

Understanding types of language models

There are various language models, each with unique strengths and ways of processing language. Most are grounded in the concept of probability distribution.

Statistical language models are the most basic form and rely on the frequency of word sequences in the textual data to predict future words based on previous words.

Neural language models, conversely, use neural networks to predict the next word in a sentence, considering a larger context and more text data for more accurate predictions. Some neural language models do probability distribution much better than others by assessing and understanding the full context of a sentence.

Transformer-based models like BERT and GPT-2 have risen to prominence for their ability to consider context before and after a word in making predictions. The transformer model architecture upon which these models are built allows them to achieve state-of-the-art results on various tasks, demonstrating the power of modern language models.

Query likelihood models are a different type of language model related to information retrieval. A query likelihood model determines how relevant a particular document is to answering a particular query.

Statistical language model (N-Gram model)

An N-gram language model is one of the foundational methods in natural language processing. Representing an advancement over unigram models based on single words and making predictions independent of any other words, the 'N' in N-gram stands for the number of words considered at a time in the model. An N-gram language model predicts the occurrence of a word based on the (N-1) preceding words. For instance, in a bigram model (N equals 2), the prediction of a word would depend on the previous word. In the case of a trigram model (N equals 3), the prediction would hinge on the last two words.

N-gram models operate based on statistical properties. They calculate the probability of a particular word following a sequence of words based on the frequency of their occurrence in the training corpus. For example, in a bigram model, the phrase "I am" would make the word "going" more probable to follow than the word "an apple," given that "I am going" is a more common sequence in the English language than "I am an apple."

While N-gram models are simple and computationally efficient, they do have limitations. They suffer from what is known as the 'curse of dimensionality,' where the probability distribution becomes sparse as the value of N increases. They also lack the ability to capture long-term dependencies or context in a sentence, as they can only consider the (N-1) preceding words.

Nevertheless, N-gram models remain relevant today and have been used in many applications, such as speech recognition, autocomplete systems, predictive text input for mobile phones, and even to process search queries. They serve as the backbone of modern language models and continue to inform the evolution of language modeling.

Neural network-based language models

Neural Network-Based Language Models, considered exponential models, represent a significant leap in language modeling. Unlike n-gram models, they harness the predictive power of neural networks to model complex language structures that traditional models fail to capture. Some models can remember previous inputs in their hidden layers and use this memory to affect the output and predict the next word or words in response more accurately.

Recurrent neural networks (RNN)

RNNs are designed to handle sequential data by incorporating "memory" of past inputs. In their essence, RNNs pass information from one step in the sequence to the next, allowing them to recognize patterns over time to help better predict the next word. This makes them particularly effective for tasks where the order of elements carries significant meaning, as is the case with language.

However, the language modeling approach is not without limitations. When sequences get too long, RNNs tend to lose the ability to connect information, a problem known as the vanishing gradient problem. A specific model variant called Long Short-Term Memory (LSTM) has been introduced to help preserve long-term dependencies in language data. Gated Recurrent Units (GRU) represent another more specific model variant.

RNNs are still widely used today, primarily due to their simplicity and effectiveness in specific tasks. However, they have been gradually supplanted by more advanced models like Transformers that offer superior performance. Nevertheless, RNNs remain foundational in language modeling and are the basis for most current neural network-based and transformer model architectures.

Transformer architecture-based models

Transformers represent a more recent advancement in language models introduced to overcome the limitations of RNNs. Unlike RNNs, which process sequences incrementally, transformers process all sequence elements concurrently, eliminating the need for sequence-aligned recurrent computation. This parallel processing approach, unique to transformer architecture, allows the model to handle longer sequences and leverage broader context in their predictions, giving them an edge in tasks like machine translation and text summarization.

At the heart of transformers are attention mechanisms that assign different weights to various parts of the sequence, allowing the model to focus more on relevant elements and less on irrelevant ones. This characteristic makes transformers exceptionally good at understanding context, a crucial aspect of human language that has been a significant challenge for earlier models.

BERT language model by Google

BERT, an acronym for Bidirectional Encoder Representations from Transformers, is a game-changing language model developed by Google. Unlike traditional models that process unique words in a sentence sequentially, bidirectional models analyze text by reading the entire sequence of words simultaneously. This unique approach allows bidirectional models to learn the context of a word based on its surroundings (left and right).

This design enables a bidirectional model like BERT to grasp the full context of words and sentences, leading to a more accurate understanding and interpretation of the language. However, the downside is that BERT is computationally intensive, requiring high-end hardware and software code and longer training times. Despite this, its performance benefits in NLP tasks such as question answering, and language inference have set new standards in natural language processing.

LaMDA by Google

LaMDA, which stands for "Language Model for Dialogue Applications," does Google develop another innovative language model. Taking conversational AI to a new level, LaMDA can generate an entire conversation given a single prompt.

It does this by leveraging attention mechanisms and some of the most state-of-the-art natural language understanding techniques. This allows LaMDA to understand grammar rules and parts of speech better, for example, and to capture subtle nuances in human conversation, such as humor, sarcasm, and emotional context, allowing it to hold conversations like a human would.

LaMDA is still in its initial stages of development, but it has the potential to revolutionize conversational AI and truly bridge the gap between humans and machines.

Language models: Present limitations and future trends

Despite their impressive capabilities, current language models still have significant limitations. One major issue is a lack of understanding of the real-world context of unique words. While these models can generate contextually relevant text, they do not understand the content they produce, a critical difference from human language processing.

Another challenge is the bias inherent in the data used to train these models. Since the training data often contains human biases, the models can inadvertently perpetuate these prejudices, leading to skewed or unfair results. Ethical concerns also arise with powerful language models, which can be exploited to generate misleading information or deep fake content.

Future of language models

Looking into the future, addressing these limitations and ethical concerns will be a vital part of developing language models and NLP tasks. Continued research and innovation are required to improve the understanding and fairness of language models while minimizing their potential for misuse.

Assuming these critical steps will be prioritized by those advancing the field, the future of language models appears promising and ripe with potential. With advancements in Deep Learning and Transfer Learning, language models are becoming increasingly adept at understanding and generating human-like text, completing NLP tasks, and understanding different languages. Transformers, like BERT and GPT-3, are at the forefront of these developments, pushing the boundaries of what's possible with language modeling and speech generation applications and helping the field delve into fresh territory, including more sophisticated machine learning and advanced applications such as handwriting recognition.

However, with progress comes new challenges. As language models become more complex and data-intensive, the need for computational resources escalates, raising questions about efficiency and accessibility. As we move forward, we aim to harness these powerful tools responsibly, augment human capabilities, and create more intelligent, nuanced, and empathetic AI systems.

The evolution of language models has been a journey marked by significant strides and challenges. The field has progressed immensely, from introducing RNNs, a language model that revolutionized how technology understands sequential data, to the emergence of game-changing models like BERT and LaMDA.

These advancements have allowed for a more profound and nuanced understanding of language, setting new standards in the field. The path forward will require ongoing research, innovation, and regulation to ensure these powerful tools are used to their fullest potential without undermining fairness and ethics.

The impact of language models on data centers

Training and operating language models require extensive computing power, putting the technology firmly in the category of high-performance computing. To handle the demands, data centers need to optimize future-enabled infrastructure and solutions for offsetting the environmental impacts of the energy consumption required to power and cool the data processing equipment that allows language models to operate reliably and without interruption.

These implications will be imperative not only for core data centers but will also impact the continued growth of cloud and edge computing. Many organizations will deploy dedicated hardware and software on-premises to support language model capabilities. Others will want to have the computing power available closer to their end users to improve the experiences that language models can offer.

In either scenario, organizations and data center operators will need to make infrastructure choices that balance the demands of the technology and the need to operate efficient and cost-effective facilities.

Explore Vertiv solutions for language models and HPC

Visit Vertiv™ Solutions and discover how we can collaborate with you to design data center power and cooling systems tailored specifically to support language model applications and other high-performance computing requirements.

PARTNERS
Overview
Consultants Corner
PARTNERS
Overview
Consultants Corner
MY ACCOUNT
Overview
Partner Login

Language & Location