Working with our Vertiv Sales team enables complex designs to be configured to your unique needs. If you are an organization seeking technical guidance on a large project, Vertiv can provide the support you require.

Learn More

Many customers work with a Vertiv reseller partner to buy Vertiv products for their IT applications. Partners have extensive training and experience, and are uniquely positioned to specify, sell and support entire IT and infrastructure solutions with Vertiv products.

Find a Reseller

Already know what you need? Want the convenience of online purchase and shipping? Certain categories of Vertiv products can be purchased through an online reseller.


Find an Online Reseller

Need help choosing a product? Speak with a highly qualified Vertiv Specialist who will help guide you to the solution that is right for you.



Contact a Vertiv Specialist

Freecooling, Evaporative and Adiabatic Cooling Technologies in Data Center Applications

The traditional cooling approach considers open aisle architectures with return air temperatures to cooling units between 22-26°C and supply air temperatures to the data center between 10-14°C to be considered standard.

With the use of intelligent air distribution management to the servers, data center designers and facility managers can increase chilled water temperatures from the standard 7-12°C, to 20-26°C.

As a result of the SmartAisle cold aisle containment solution, the servers’ exact cooling and airflow needs are met, thus investing only necessary kilowatts in targeted cooling. The SmartAisle solution increases space efficiency and provides uniform and predictable temperature to all IT equipment, directly controlling cold aisle temperature and humidity.

Combined with the right chiller, such as the Liebert® HPC freecooling chiller or the Liebert AFC adiabatic freecooling chiller, the benefits are even greater:

  • Higher capacity at smaller footprint
  • Significant energy savings as a result of the freecooling usage for a significant number of hours per year
  • Low noise operation

In this paper, we will investigate the impact of using freecooling technologies with and without adiabatic and evaporative technologies in major EMEA cities.

Related Articles

PARTNERS
Overview
Consultants Corner
PARTNERS
Overview
Consultants Corner
MY ACCOUNT
Overview
Partner Login

Language & Location